This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3000 Smart configuration problem

Hi,

       The cc3000 Device is connecting to the access point with smart configuration. But In my application, after some time the device has to disconnect from the previous access point and it has to connect to the another access point. But CC3000 is not coming out from the smart configuration mode. I am using the wlan_disconnect() API  to disconnect from the previous access point. It is disconnecting and automatically connecting to the same access point which is given by the smart configuration.

How to exit form the smart configuration mode. wlan_smart_config_stop() API also not working to exit from the configuration mode. So any one Please help to solve this issue.

Regards,

KC.

  • Hi,

    I solved this issue. After WiFi Smart Configuration, WiFi Connection Policy API Function Should be change to wlan_ioctl_set_connetion_policy(0,0,1), after disconnecting the CC3000, Reset the CC3000, Reinit the CC3000, again change the  WiFi connection policy to  wlan_Ioctl_set_connetion_policy(0,0,0)

    Thanks,

    KC.