Hi all,
I am running SP 1.24 and configing the CC3000 to use DHCP. I connected to an AP on network A and I receive an IP address, Gateway, Netmask, and DNS Server address. All ok.
Now I move to network B. Connect again. This time netapp_ipconfig returns my details but the DNS server is THE SAME as on the previous network (even though it is not really, in fact the network portion of the address are different on these two networks.
It is as if the DNS server address was remembered from the previous network. Also DNS didn't work (which it shouldn't of course if the DNS address which the device is using is wrong)/
Any ideas about this mystery.
Thanks
Ciarán