Hello,
I'm a bit lost with documentation. I'm develloping an access control application with an embedded module, CC3000.
What I'm confused is about the storing of the network parameters. Each time I reset or power up CC3000 module do I need to send to the module the network parameters (SSID string, encryption mode WEP WPA, encription key, etc) or are they stored in CC3000 EEPROM?
This is an important issue as I will need or not need to have an external EEPROM to store these parameters.
I'm finishing hardware design and this is the last issue in my project.
Best regards,
Vitor Barbosa