This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3000 Timeout issue

Hi,

I have recently upgraded  cc3000 firmware from 1.10 to 1.24  ,after update I can see firmware 1.24.

Small application  displays SSIDs available . but when I tried to connect with any of the SSID. Module returns Timed out.( i.e. it is not able to connect to SSID).

I was able to connect before upgrade. with same module. any help is appreciated.

Here are the debug output messages, when debug mode enabled.

---------------------------------------------

.TX Buffer : 131 bytes
.Free RAM: 1227
..Initialising the CC3000 ...
..CC3000: init_spi.
.CC3000: Finished init_spi.
init.
start.
.CC3000: SpiOpen.CC3000: WlanInterruptEnable..
.CC3000: Finished SpiOpen.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: WriteWlanPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin - 001.
.CC3000: ReadWlanInterruptPin


Thanks
Naveen