Hello,
I have one more query related the standard pinout for
TM4c123GXL Launchpad with CC3000 is
given as below,
For Tiva For CC3000
1 Vcc Vbat
2 PB5 Vbat_EN
3 PB0
4 PB1
5 PE4
6 PE5
7 PB4 WI_SPI_CLK
8 PA5
9 PA6
10 PA7
11 PA2
12 PA3
13 PA4
14 PB6 WI_SPI_DOUT
15 PB7 WI_SPI_DIN
16 RST
17 PF0
18 PE0 WI_SPI_FSS
19 PB2 WI_SPI_IRQ
20 GND GND
I have some doubt here that pin 2 SPI_fss for board TM4C123GXL is
connected to CC3000 pin 2 which is Vbat enable and CC3000 has pin 18 which is Wi_SPI_Fss
which is exactly mismatch as per pins mention in EK-TM4cGXL Lanuchpad
& Swru331 pdf. So user need to change in hardware by ext connection to
configure SPI_fss pin for TM4c