This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Maximum current needed to operate Wilink 8 modules at 1.8V I/O domain

Other Parts Discussed in Thread: WL1801MOD, BL6450

Hi Champs!

We want to operate both  BL6450 , and WL1801MOD in 1.8V I/O domain . could you please let us know the maximum current required for VDD(3.3V) and VDDIO(1.8V) for both Bluetooth and combo module.

Can you please clarify?

Best Regards

Feroz

  • Hi Feroz,

    You should be able to find this information in the datasheet.

    Regards,
    Gigi Joseph.

  • Thanks Gigi!

    However I am not 100% sure if the VDD can be operated at 3.3V and VDD-IO at 1.8V....is the setting even for the tables...

    Would section "WLAN Currents" be the right data for this?

    WLAN Currents
    Specifications Items Typ (avg) – 25°C Units
    Receiver Low-power mode (LPM) 2.4-GHz RX SISO20 single-chain 49 mA
    2.4 GHz RX search SISO20 54 mA
    2.4-GHz RX search MIMO20 74 mA
    2.4-GHz RX search SISO40 59 mA
    2.4-GHz RX 20 M SISO 11 CCK 56 mA
    2.4-GHz RX 20 M SISO 6 OFDM 61 mA
    2.4-GHz RX 20 M SISO MCS7 65 mA
    2.4-GHz RX 20 M MRC 1 DSSS 74 mA
    2.4-GHz RX 20 M MRC 6 OFDM 81 mA
    2.4-GHz RX 20 M MRC 54 OFDM 85 mA
    2.4-GHz RX 40 MHz MCS7 77 mA
    Transmitter 2.4-GHz TX 20 M SISO 6 OFDM 15.4 dBm 285 mA
    2.4-GHz TX 20 M SISO 11 CCK 15.4 dBm 273 mA
    2.4-GHz TX 20 M SISO 54 OFDM 12.7 dBm 247 mA
    2.4-GHz TX 20 M SISO MCS7 11.2 dBm 238 mA
    2.4-GHz TX 20 M MIMO MCS15 11.2 dBm 420 mA
    2.4-GHz TX 40 M SISO MCS7 8.2 dBm 243 mA