Hi..I am attempting using the CC3000 module by directly connecting it to MSP-EXP430G2. I wanted to know if we can connect cc3000 module to the MSP-EXP430G2 directly instead of using the CC3000 boost? I did the connections using its pin discriptions and tried running the basic Wi-Fi application. There seems to be some error in recieving data from CC3000. The hyperterminal window opens but doesn't display anything. I hooked it up to a CRO. The data seems to transmitting from MCU to CC3000 but the response from cc3000 to MCU is low after 24 clock cycles and becomes high only after all the clock cycles are completed. Please do help in any way possible. Thanks