This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x + WL18xx Slow Clock options

Other Parts Discussed in Thread: WL1835MOD

Hi,

looking at both COM8 with WL1835MOD and BB WL1835MOD cape, schematics in both cases we connect a 32.768kHz oscillator to WL8.

 

The AM335x has a 32.768kHz Crystal as the RTC clock input and can output that clock on CLKOUT2. The specs for the crystal on the AM335x are a range of 20 ... 50ppm jitter and I am assuming that this jitter would make it out on CLKOUT2.

Could the WL18xxMOD be driven directly from CLKOUT2, instead of a separate 32.768kHz oscillator?

Are there any concerns with this?

 

Thanks,

--Gunter

 

  • Hi all,

    the reason why we are concerned driving WL18xx from CLKOUT2 32.768kHz source are some statements made in the AM335x TRM

    4.2.4 Output Clock Characteristics

    NOTE

    The AM335x CLKOUT1 and CLKOUT2 clock outputs should not be used as a synchronous

    clock for any of the peripheral interfaces because they were not timing closed to any other

    signals. These clock outputs also were not designed to source any time critical external

    circuits that require a low jitter reference clock. The jitter performance of these outputs is

    unpredictable due to complex combinations of many system variables. For example,

    CLKOUT2 may be sourced from several PLLs with each PLL supporting many configurations

    that yield different jitter performance. There are also other unpredictable contributors to jitter

    performance such as application specific noise or crosstalk into the clock circuits. Therefore,

    there are no plans to specify jitter performance for these outputs.

    Another data point is that no AM335x designs drive the 32kHz clock directly from the SOC, but have separate oscillators.

     

    With the above, could the WL8 team comment?

     

    Thanks,

    --Gunter

     

     

  • Hi all,

    do you have an update on the above question? It has been out there for a while.

     

     

    Thanks,

    --Gunter