Hi,
About certifications for WL1837 2.4 + 5G.
1. EN301893 only specifies 5150~5725MHz, while band4 need to use EN302502 or EN300440.
As the WL1837 can use of band (5725~5850MHz), what standard would be recommended to choose here?
For example, on the TI certified WL18xx modules, what is actually tested here?
2. FCC seems to have special rules for "master device" (which I assume is AP)
Then so called DFS testing needs to be done by FCC. Is this really mandatory for running an access-point (or wifi-direct) at 5G?
Thanks David