Other Parts Discussed in Thread: MSP430FR5739
Dear TI supporter ,
We try follow the wiki suggestion and load the patch as below(blue word procedure) . But the result is only LED5 turns on, that means the patch on both firmware and driver is not successful to load on the CC3000MOD.
Do you have any idea, what's going wrong from us ?
Thanks
Roderick
Burning the patches to the module is also available with a binary file. In order to burn the patches using executable binary follow these instructions:
Open Start -> All Programs -> CC3000 Patch Programmer -> MSP430FR5739 -> Download Driver Patches
LED5 and LED8 turn on upon successful completion.
If LED1 turns on as well, it indicates a missing MAC address.
Open Start -> All Programs -> CC3000 Patch Programmer -> MSP430FR5739 -> Download Firmware Patches
LED5 and LED8 turn on upon successful completion.