This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cost of CC3100 and CC3200

Other Parts Discussed in Thread: CC3100

What will be the approximate cost of these two chips per 1ku? I just need a ballpark figure.

  • Ivor: in the future I would recommend combining both your questions into the same post.

    To answer both, the availability date has not been released by TI -- however, the Launchpad is available for order through their WebShop, so it can't be too far off. The chip itself is generally not available until a while after the Launchpad has been circulating, if the Tiva C is any indication (unless you're a big company that TI partners with, but if you were you'd already know the answer).

    As far as price, any answer would surely be speculation. We'll just have to wait and see. Keep checking the TI main website, at the CC3100 page, and also check their distributors (ie Newark, Mouser)

  • Hi Alexander,


    Thanks for answering my post, but the information that you have is pretty much what I was able to gather from TI's website. I would be happy if someone from TI who has more specific information and is allowed to share it can answer.

  • This line hasn't even 'officially' been launched; the information on the website is mostly still in preview stage. None of the TI employees will be able to release any more information until after the official launch.

    To be honest, I was surprised the SDK was available for download. I have a feeling it won't be too long until the rest of the software and info is ready.

  • It was definitely launched in "Preview" mode a couple of days ago. When is it going to be available in "Active" mode is another question that I asked in another thread.

    I think this information is very important to early adapters at this stage, since it helps one decide whether to be an early adapter or not. It is definitely in TI's interest to release this information sooner rather than later, since they will gather more early adapters, which in turn will help clean out bugs sooner as well as get more exposure. The two unknowns (price and general availability) are definitely preventing me from getting on the early adapter band wagon right now and I am guessing its preventing others as well.

    As far as official announcements go, TI has not been very proactive in this department. For example when the latest version of the CC3000 firmware was released, there was no official announcement whatsoever.

  • All,

    We will be sharing more details on these exciting new products very soon. Please stay tuned and thanks for your interest.

     

    Adnan

  • The CC31xx and CC32xx products are officially released on June 16th!

    http://newscenter.ti.com/2014-06-16-Add-Wi-Fi-to-anything-with-TIs-Internet-on-a-chip

    Connect More. Anywhere. Anything. Anyone.

    All the best!

  • All,

    We are please to annouce earlier today, the new SimpleLink™ Wi-Fi family delivering the industry's first single-chip, low-power Wi-Fi solution with built-in programmable MCU designed for the IoT. You can find more informaiton on this exciting new product including pricing and availability in the annoucement below: