Hey Team,
Is the CC3200 capable of over the air updates to the firmware? My thoughts were yes. I was thinking you could establish a connection to an FTP server pull down the update to SFLASH and then instruct the bootloader to load that code on the next restart. As long as the device has the correct SOP setting of 0x000 which would instruct the bootloader to load the application image from SFLASH to internal MCU RAM. Is this the correct way of thinking of this? One thing I’m unsure of is if the application processor has access to write the SFLASH?
Thank you in advance
-Jason