Other Parts Discussed in Thread: MSP430G2553
Hello,
I am new to the CC3000 platform. I am using Launchpad MSP430G2553 with CC3000 boosterpack.
I am trying to run the Basic Wifi Application from the CC3000 SDK.
I have followed the instructions listed in:
http://www.ti.com/lit/ml/slab067/slab067.pdf
1) Run the Patch Programmer for Driver and Firmware update on CC3000
2) Download the Wifi Application
(both for MSP430G2553)
When I launch my Serial Putty Session (with all okay parameters) after reset I see on Putty Serial Terminal:
Example App:driver version 2.13.7.15
However, when I type 03 and enter, I do not see a ``DONE'' output, and the device seems to be stuck.
If I reset,
I again see
Example App:driver version 2.13.7.15
If I now type 0 and enter, I get
Illegal command
DONE
What's happening? Why don't I get a DONE when I type 03. None of the legal commands, 01,03... seems to get any DONE signal.
Please help.
Vishal.