We are using Murata module (LBEL1CESEC) with WiLink7. All application notes have been followed for HW integration. Power rails and TCXO have been thoroughly tested (tolerance, stability, jitter, PN, signal quality, power rail, power rail noise, etc) and meet WL1281 specs where relevant. System is operational but has a GPS transient speed bump issue - sudden peaks of speed are reported incorrectly - they correlate closely to transients in the reported parameter "Clock Frequency Bias" related to the TCXO.
NAVD software we are using:
version.h:#define SW_VERSION_STR "NaviLink_MCP2.6_RC1.12"
version.h:#define NAVC_VERSION_STR "Navilink_MCP2.6_BL2.0.14"
We do not understand what the parameter "Clock Frequency Bias" really means. It is reported in m/s but TCXO frequency is cycles/s. Can someone explain please. We feel our TCXO circuit is stable and clean but would like to check anything that could lead us to resolve this issue.
Is there anything we could or should measure or investigate in the hardware that could cause this phenomenon.