whether are there some patch or user guide to introduce how to run BlueZ on WL1835, I am using the AM335x SDK6.0 ?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
whether are there some patch or user guide to introduce how to run BlueZ on WL1835, I am using the AM335x SDK6.0 ?
Thanks!
Hi,
Yes it is possible. please follow the below link http://processors.wiki.ti.com/index.php/Open_Source_Wireless_Connectivity_WiLink8_Build_scripts
Mind that SDK6.0 uses Linaro toolchain which is part of the SDK
I am following this guide, when i compile it, there are many many error;
are you sure that the user guide is ok?
Hi,
As mentioned earlier SDK6.0 uses Linaro toolchain which is part of the SDK. which should be used instead of the Arago tool chain mentioned in the link provided.
other than that it should work.
Please also go through the "sitara-linuxsdk-sdg-06.00.00.00.pdf" from the below link
http://software-dl.ti.com/sitara_linux/esd/AM335xSDK/06_00_00_00/index_FDS.html
There is virtually nothing on the given page http://processors.wiki.ti.com/index.php/Open_Source_Wireless_Connectivity_WiLink8_Build_scripts
History mentions something about moving to or from the page - not clear on what this means. Where is he new page - this is not clear.