Hi,
I am getting below panic while loading wifi module for imx6 solo board.
wl1271: ERROR watchdog interrupt received! starting recovery.
wl1271: Reading FW panic log
wl1271: ERROR command complete timeout
------------[ cut here ]------------
WARNING: at /home/vishwa/ti-compat-wireless-wl12xx-0.20120206r412_02/drivers/net/wireless/wl12xx/cmd.c:107 wl1271_cmd_send+0x38c/0x3d
4 [wl12xx]()
Modules linked in: wl12xx_sdio wl12xx mac80211 cfg80211
[<8003e7e8>] (unwind_backtrace+0x0/0xf8) from [<8006a240>] (warn_slowpath_common+0x4c/0x64)
[<8006a240>] (warn_slowpath_common+0x4c/0x64) from [<8006a274>] (warn_slowpath_null+0x1c/0x24)
[<8006a274>] (warn_slowpath_null+0x1c/0x24) from [<7f091398>] (wl1271_cmd_send+0x38c/0x3d4 [wl12xx])
[<7f091398>] (wl1271_cmd_send+0x38c/0x3d4 [wl12xx]) from [<7f091558>] (wl12xx_cmd_stop_fwlog+0x54/0x80 [wl12xx])
[<7f091558>] (wl12xx_cmd_stop_fwlog+0x54/0x80 [wl12xx]) from [<7f090058>] (wl1271_recovery_work+0x1b4/0x2d0 [wl12xx])
[<7f090058>] (wl1271_recovery_work+0x1b4/0x2d0 [wl12xx]) from [<8007effc>] (process_one_work+0x10c/0x38c)
[<8007effc>] (process_one_work+0x10c/0x38c) from [<8007f834>] (worker_thread+0x170/0x37c)
[<8007f834>] (worker_thread+0x170/0x37c) from [<800836e4>] (kthread+0x80/0x88)
[<800836e4>] (kthread+0x80/0x88) from [<80038aa4>] (kernel_thread_exit+0x0/0x8)
---[ end trace 4e6ab4fb8eff15af ]---
wl1271: ERROR failed to send stop firmware logger command
First address of fwlogger = 0x2603
wl1271: Hardware recovery in progress. FW ver: Rev 6.3.3.0.79 pc: 0x29cc
wl1271: down
ieee80211 phy0: Hardware restart was requested
wl1271: firmware booted (Rev 6.3.3.0.79)
wl1271: Driver version: R4_SP2_03_00
wl1271: Association completed.
wl1271: ERROR no active RX BA session on tid: 0
Need some way to resolve this.
Thanks,
Subhaprada