Hi,
We are trying to get the wl18xx (wl1835) to use both antennas for 2.4 GHz WLAN.
The board has 2 antennas for 2.4 GHZ, none for 5 GHz.
When ever we connect using a SISO device, only ANT1 is used. We've tested with wl18xx.ht.mode = 0x00 (MIMO) and wl18xx.ht.mode = 0x02 (SISO20).
Is it possible to get the two antennas to work together so that the module always uses the antenna with the best signal ?
- in other words, we are not interrested in multiple streams (MIMO), but one stream (SISO) from the antenna with the best signal.
Thank you.
BR, David