Hi,
I've recently started working with the CC3000 booster pack connected to a MSP430G2553. I followed the instructions found here using the Basic Wi-Fi application
I was able to connect to my mobile phone AP using the command
028godzilla
and getting the response
DONE
IP:192.168.43.103
after this I try to open a socket using the command
03
and get the response
Illegal Command
DONE
also try to disconnect using the command
09
and am met with the same Illegal command DONE response. I am unsure of why this occurring.
I am using Docklight V2.0 as my terminal program and see no error in communication. Is there something that I have overlooked in the code and need to change? I appreciate any help you're able to give.
Regards,
Luke.