I've attempted running the "Wifi Starter" iOS source code from Xcode 5 and I get the errors listed at the bottom of this post. I think the root problem seems to be the first warning. Apparently Xcode 5 is ignoring the FirstTimeConfig library because it is missing a required i386 architecture. I'm not sure what this means. Has anyone else successfully launched the application from Xcode? Has anyone else seen this problem? I'm running Mavericks.
ld: warning: ignoring file /Users/jacksonkeating/Documents/Example Code/WiFi_Starter_App_iOS_Source_1.0/Source/SmartConfigCC31XX/libFirstTimeConfig.a, missing required architecture i386 in file /Users/jacksonkeating/Documents/Example Code/WiFi_Starter_App_iOS_Source_1.0/Source/SmartConfigCC31XX/libFirstTimeConfig.a (3 slices)
Undefined symbols for architecture i386:
"_OBJC_CLASS_$_FirstTimeConfig", referenced from:
objc-class-ref in SmartConfigSCViewController.o
ld: symbol(s) not found for architecture i386
clang: error: linker command failed with exit code 1 (use -v to see invocation)