Hi all,
I am new to the launchpad but not really new to the Cortex M family since i have done a couple of projects in STM32F4 using Keil. So please bear with me..
I find using the SFLASH a bit weird since i was used to having an in built Flash in the uControllers and having an external flashing tool to save into the SFLASH mem was kinda new. And i had no idea what the SOP jumpers were for. I was lost for 1 full day(yes, 24 hours) but this forum saved me. This forum really provides a wealth of info.
I seem to encounter this problem only during debugging mode. IAR flashes a dialog box as such. The thing is i have no idea why the path points to the mentioned directory.. Ignoring the messsage allows me to step through but sometimes somewhere down there will be another pop up with a path pointing tp cpu.c file.
I am able to download to SFLASH using UNIFLASH(SOP jumper on and then removed) and run in SRAM(exiting debug w/o pressing the reset button) with no problem. The 3 LEDs blink.
However this massage annoys me when i debug. I can skip it but that's not the point... Any help is appreciated..