I want to use the WL1803MOD with external antennas. The external antenna is connected to the board with a U.FL connector. Can I connect the U.FL connector via a 50ohm circuit direct to module antenna output or must there be placed compensation compnents. If there have to be compensation components, where can I find information about the calculation ?
Best regards
Johan