Hi,
I am using AM335x EVM connected with WL1835MOD. I am using Bluetopia platform manager for SPP communication between EVM and other devices. In my application, the evm continuously receives data every 1ms. When this happens, I sometimes see the following error,
(stc): chip/interface misbehavior dropping frame starting with 0x01(stc): chip/interface misbehavior dropping frame starting with 0x00
(stc): chip/interface misbehavior dropping frame starting with 0x00(stc): chip/interface misbehavior dropping frame starting with 0x001
The baud rate set is 3000000.
What could be the reason for this? Is it due to fast reception of data?
Regards,
Harini