Please tell us about the CC3100 / CC3200.
(1) Do you have any data about the communication distance?
(2) For throughput, It has become to the following description in the data sheet. TCP: 12Mbps UDP: 16Mbps
How much has been confirmed in the measured value?
(3) If you turn on the encryption process, Is there a change in the communication rate?
(4)I think that CC3100 / CC3200 and can transmit data of 1460 bytes by issuing once sl_send command.
When transmitting the data of 1460 bytes or more, I need to issue many times sl_send command?
Best Regards,
hamada