Hi Folks,
How can be connect the CC3100 application to the internet? we can create an access point with the help of cc3100 and connect say a mobile to it. How can we connect the CC3100 to the web and surf the Internet through the Mobile.
Srijan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Folks,
How can be connect the CC3100 application to the internet? we can create an access point with the help of cc3100 and connect say a mobile to it. How can we connect the CC3100 to the web and surf the Internet through the Mobile.
Srijan
Srijan,
This is not supported w/ our device today.
-Praneet
Alternatively suggest following :
1. Enable hot spot on your mobile.
2. Connect CCC3100 ( in STA mode) to you mobile.
3. CC3100 can access internet while you can continue browsing the net thru your mobile.
Regards,
Geet
Hello all,
I want to configure CC3100 as a webserver so that I can access the pages from Internet from anywhere in the world. The board acts a server if I connect a station (say a Laptop or Cellphone) to the AP of CC3100 but this configuration is like LAN, I want to extend it to internet so that the pages stored on CC3100 can be accessed from internet.
Kindly help me with this.
Thanks
Ashwin Deshpande
David,
I am closing the thread - Please open a new thread (and add a link to this thread for reference) if the issue still persists or additional information is required.
-Praneet