This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL18xx firmware fits EN 300 328 v1.8.1?

Dear Sirs:

  We are using WL18xx module to design our product. However our customer ask to confirm that not only the H/W but also the F/W can fit ETSI EN 300 328 v1.8.1.

  Per the discussion http://e2e.ti.com/support/wireless_connectivity/f/307/p/339339/1185917.aspx#1185917

The WIFI firmware R8.4 fits ETSI EN 300 328 v1.8.1.

  Just for sure, if we are using firmware R8.3SP1, the above discussion implies that we need to move R8.4 to comply the ETSI EN 300 328 v1.8.1.

  Is my understanding correct?

Regards,

/ckhsu