Hello,
I am developing an application with CC3200 and I would like to get a CC31xx_antenna_diversity_board
Where could I purchase it ?
Thank you very much
Best Regards
Joseph
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks Adnan,
I'm waiting for you;
Please can you send us the schematics ?
Best Regards
Joseph
Hi Adnan,
Just trying to understand the antenna diversity booster schematic. In my application, if I want to design the use of a chip antenna as the main antenna but have an alternative U.FL connector for situations where extra range is needed, would I need to add an RF switch like the SKY13351-378LF used on the antenna booster board, then use the antenna selection GPIOs to allow the software to switch between the two? What's the purpose of U4 and U6,U7?
Evan
Hi,
Executing the antenna diversity exemple programm,with my own hardware,all seems to work fine with NOTERM. But, when I flash without NOTERM symbol, it doesn't work.
I have to work with serial port for debugging.
Can anybody help me ?
Is it parameters issues from uniflash ?
Many thanks
Joseph