Hi,
I was trying the Exosite Cloud Demo Example Program and I thought I did not load the binary at my CC3200 Launchpad, because of this error message below at Uniflash. I tried several times with the same results thinking that the binary was not loaded at my CC3200 Launchpad. But, upon confirmation the binary was loaded and I was able to test the Exosite Cloud Demo Example Program.
I am just new to Uniflash for CC3200 and not much familiar with the logs so I got confused. Is there a guide that will help new guys interpret these Uniflash logs better?
Binary still loaded Uniflash log:
[18:53:33] INFO: > Updated Token value: 0x0
[18:53:33] INFO: > File name: /cert/ca.pem, Update: true, Erase: true
[18:53:33] INFO: > Erase File: /cert/ca.pem
[18:53:33] INFO: erasing file "/cert/ca.pem"
[18:53:33] INFO: deleting file "/cert/ca.pem"
[18:53:34] INFO: erase file completed
[18:53:34] FATAL: > File "location on local machine" does not exist on local File System
[18:53:34] INFO: > Executing Operation: Disconnect
[18:53:34] Operation Program returned.
- kel