Can a JLink be used to debug the CC3200 with CCS v6.0.1?
I've seen a post that says it's only supported in CCS v5.x, but can't find anything about v6. I'm also using the CCS Free License with the SimpleLink Launch XL Board will this be an issue?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can a JLink be used to debug the CC3200 with CCS v6.0.1?
I've seen a post that says it's only supported in CCS v5.x, but can't find anything about v6. I'm also using the CCS Free License with the SimpleLink Launch XL Board will this be an issue?
Not 100% sure if the JLink will be fine for debugging the CC3200, but I suspect it should not be a problem...so long as CCS supports it. You might want to ask the CCS forum to confirm - http://e2e.ti.com/support/development_tools/code_composer_studio/f/81.aspx
However, you will need the full version of CCS to use this emulator. The only emulator that will work on the Free version is the budget XDS100, which you can order for about $80 from the TI eStore.
Glenn.
Hello all,
As per the link below, J-Link is not supported on CCS 6.x:
http://processors.wiki.ti.com/index.php/J-Link_Emulator_Support
Thanks,
Sem Amesawu