I am testing a CC3200 Launchpad XL with an external antenna, and the RSSI that I am measuring is 16 dB worse than the RSSI that I measure with the chip antenna.
The only thing that I did to switch from a chip antenna to an external antenna was to rotate R111 90 degrees and solder it in place of R110. Do I need to take other steps to switch to the u.fl socket?
I'm noticing the component L8 that is not placed on the board. Does that need to be matched to the antenna I am using?
I've tried several different quarter-wave antennas and dipole antennas, but the results are all significantly worse than when the board is configured for the chip antenna.