Hi all,
Yesterday I got the CC3200 launchpad (Rev 3.2) and messed around a bit with the preloaded demo app. Everything worked fine. I followed the instructions in the getting started guide to set up the tool chain. I'm using ccsv6. I managed to flash and run the httpserver example so I could see the debug output in tera term. For some strange reason - I haven't connected anything to the board neither changed the jumper settings - the third or fourth time I tried to flash ccs gave me the error message "couldn't connect to target". Rebooting didn't help so I tried to do a "get version" in uniflash but without success. Uniflash prints:
[11:13:37] INFO: setting break signal
[11:13:37] INFO: --- please restart the device ---
[11:13:52] ERROR: ---reading ACK signal failed---
I saw that others are having the same problem so I followed the advices in this and this thread and could ensure that the ftdi chip is working correctly. I can see actions on the uart_rx line (J6) but no (re)actions on the uart_tx line (J7). The tx line remains low all the time. I of course quadruple-checked the jumper settings so this can't be the problem. Then I had a look on the communication lines of the sflash and since there nothing happened after a device reset (even with SOP set to 000), I have to assume my device is already in heaven.
But.. why?
Reading the threads mentioned above showed that others have broken their devices too without having any idea how and short after they got the device.
Are there any known issues with this chip (its an xcc3200hz)? Could I accidently have corrupted the bootloader in some way?
Any advice is appreciated!
Thanks in advance,
Michael