Hi,
I cannot use UniFlash to Format my CC3200-LAUNCHXL(Rev 3.2). The Console output is below:
[19:14:29] Begin Format operation. [19:14:29] INFO: > Executing Operation: Connect [19:14:31] INFO: setting break signal [19:14:31] INFO: --- please restart the device --- [19:14:46] ERROR: ---reading ACK signal failed--- [19:14:48] INFO: setting break signal [19:14:48] INFO: --- please restart the device --- [19:15:03] ERROR: ---reading ACK signal failed--- [19:15:05] INFO: setting break signal [19:15:05] INFO: --- please restart the device --- [19:15:20] ERROR: ---reading ACK signal failed--- [19:15:23] INFO: setting break signal [19:15:23] INFO: --- please restart the device --- [19:15:38] ERROR: ---reading ACK signal failed--- [19:15:38] FATAL: --- Can't connect to device !! --- [19:15:38] FATAL: Error connecting to the device. Please check your COM port settings. Error code: -3 [19:15:38] INFO: > Executing Operation: Disconnect [19:15:38] Operation Format returned.
And I tried to press the Reset button to restart the device, but it seems no use at all.
For the other options, e.g. Program, Service Pack Update, and Get Version, all failed similarly.
What I had done is not clear even to me, due to that time I tried to learn how to make it run. I might use UniFlash to "Get Version" because it seems safe. And maybe I connect my Xshell with the COM port at the same time... I can guarantee that the hardware should not have issue, I myself is an electronics engineer.
I just want to know, how to fix my board? Or is it corrupted?
What is the biggest potential issue? Which component may be damaged? I can change some one by manually soldering a new one.
Thanks!
More:
I bought another CC3200-LAUNCHXL board, and I can program simple code onto it. So I know the basic operration of this board (e.g. the setting of the jumpers) and UniFlash.