Hi All,
I am trying to run wlan_station example on CC3200 lanchxl using code composer, and with the help of "CC3200 SimpleLink™ Wi-Fi® and IoT Solution With MCU LaunchPad™ Getting Started Guide".
I was able to build the projects, but when running it in Debug mode it doesn't connect.
I get the following error:
Cortex_M4_0: Trouble Reading Memory Block at 0x20030008 on Page 0 of Length 0x4: Debug Port error occurred.
And in the Tera term:
*************************************************
CC3200 WLAN STATION Application
*************************************************
Host Driver Version: 1.0.0.1
Build Version 2.0.7.0.31.0.0.4.2.1.5.3.3
Device is configured in default state
Device started as STATION
Error [-3] at line [761] in function [WlanConnect]
Failed to establish connection w/ an AP
Any Idea?
Best Regards
Ilan