This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL18xx Wifi and BT not working in custom board

Other Parts Discussed in Thread: TPS65910

Hi,
We've built a custom board with Am335x+WL18xx. The WL18xx is connected in UART2 as opposed to UART1 in the EVM board. We've made the necessary changes for this and when we launched the BT app, we get the below error:

SPPM>1 1'^H

BTPM_Initialize() Success: 0.
DEVM_RegisterEventCallback() Success: 5.
SPPM> ^H

Invalid Command.
SPPM>9

Usage: SetDevicePower [0/1 - Power Off/Power On].
Function Error.
SPPM>9 1

DEVM_PowerOnDevice() Failure: -14, Unknown Error.
Function Error.
SPPM>

Also WLCore driver is not getting loaded. SDIO is connected in MMC2.

I'm attaching the dts file we've used (SDK 7.0) and the Kernel boot log. It is attached as zip file.

Can you please let us know what could be the issue?

I'm pasting the log for quick reference:


Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 3.12.10-ti2013.12.01 (root@labubuntu-Sanmina) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #34
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: Generic AM33XX (Flattened Device Tree), model: TI AM335x EVM
[ 0.000000] cma: CMA: reserved 24 MiB at ae000000
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 259856
[ 0.000000] Kernel command line: console=ttyO1,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1003116K/1045504K available (5567K kernel code, 559K rwdata, 1884K rodata, 345K init, 225K bss, 42388K reserved, 267264K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xef800000 ( 760 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc074f04c (7453 kB)
[ 0.000000] .init : 0xc0750000 - 0xc07a6638 ( 346 kB)
[ 0.000000] .data : 0xc07a8000 - 0xc0833fd8 ( 560 kB)
[ 0.000000] .bss : 0xc0833fd8 - 0xc086c780 ( 226 kB)
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
[ 0.000000] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000000] Console: colour dummy device 80x30
[ 0.000295] Calibrating delay loop... 663.55 BogoMIPS (lpj=3317760)
[ 0.049747] pid_max: default: 32768 minimum: 301
[ 0.049846] Security Framework initialized
[ 0.049892] Mount-cache hash table entries: 512
[ 0.056728] CPU: Testing write buffer coherency: ok
[ 0.057147] Setting up static identity map for 0xc0575868 - 0xc05758d8
[ 0.057967] devtmpfs: initialized
[ 0.059498] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.060768] ------------[ cut here ]------------
[ 0.060813] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_hwmod.c:2574 _init+0x4c8/0x520()
[ 0.060821] omap_hwmod: i2c2: doesn't have mpu register target base
[ 0.060828] Modules linked in:
[ 0.060843] CPU: 0 PID: 1 Comm: swapper Not tainted 3.12.10-ti2013.12.01 #38
[ 0.060850] Backtrace:
[ 0.060872] [<c0017880>] (dump_backtrace+0x0/0x10c) from [<c0017a1c>] (show_stack+0x18/0x1c)
[ 0.060880] r6:c075d11c r5:00000009 r4:ed083e30 r3:00000000
[ 0.060906] [<c0017a04>] (show_stack+0x0/0x1c) from [<c056de50>] (dump_stack+0x20/0x28)
[ 0.060927] [<c056de30>] (dump_stack+0x0/0x28) from [<c0046d08>] (warn_slowpath_common+0x70/0x90)
[ 0.060941] [<c0046c98>] (warn_slowpath_common+0x0/0x90) from [<c0046dcc>] (warn_slowpath_fmt+0x38/0x40)
[ 0.060946] r8:c075d638 r7:00000000 r6:c075cc54 r5:c07b5698 r4:c07db4dc
[ 0.060965] [<c0046d94>] (warn_slowpath_fmt+0x0/0x40) from [<c075d11c>] (_init+0x4c8/0x520)
[ 0.060971] r3:c06a61a4 r2:c069f468
[ 0.060993] [<c075cc54>] (_init+0x0/0x520) from [<c002dcac>] (omap_hwmod_for_each+0x38/0x64)
[ 0.061007] [<c002dc74>] (omap_hwmod_for_each+0x0/0x64) from [<c075d664>] (__omap_hwmod_setup_all+0x2c/0x48)
[ 0.061013] r7:c0750410 r6:c0834000 r5:00000001 r4:c07a5cbc
[ 0.061032] [<c075d638>] (__omap_hwmod_setup_all+0x0/0x48) from [<c00089ec>] (do_one_initcall+0xf4/0x154)
[ 0.061055] [<c00088f8>] (do_one_initcall+0x0/0x154) from [<c0750b94>] (kernel_init_freeable+0xf0/0x1bc)
[ 0.061069] [<c0750aa4>] (kernel_init_freeable+0x0/0x1bc) from [<c0568b08>] (kernel_init+0x10/0xec)
[ 0.061092] [<c0568af8>] (kernel_init+0x0/0xec) from [<c00146f8>] (ret_from_fork+0x14/0x3c)
[ 0.061098] r4:00000000 r3:00000000
[ 0.061151] ---[ end trace 1b75b31a2719ed1c ]---
[ 0.119825] omap_hwmod: debugss: _wait_target_disable failed
[ 0.120542] pinctrl core: initialized pinctrl subsystem
[ 0.121314] regulator-dummy: no parameters
[ 0.123762] NET: Registered protocol family 16
[ 0.125667] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.127850] cpuidle: using governor ladder
[ 0.127862] cpuidle: using governor menu
[ 0.134358] platform mpu.1: FIXME: clock-name 'fck' DOES NOT exist in dt!
[ 0.135250] platform 49000000.edma: FIXME: clock-name 'fck' DOES NOT exist in dt!
[ 0.136300] OMAP GPIO hardware version 0.1
[ 0.143271] platform 56000000.sgx: FIXME: clock-name 'fck' DOES NOT exist in dt!
[ 0.145408] DSS not supported on this SoC
[ 0.145425] No ATAGs?
[ 0.145436] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.163755] bio: create slab <bio-0> at 0
[ 0.175301] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.176051] vbat: 5000 mV
[ 0.176510] wlan-en-regulator: 1800 mV
[ 0.178835] vgaarb: loaded
[ 0.179999] SCSI subsystem initialized
[ 0.181122] usbcore: registered new interface driver usbfs
[ 0.181263] usbcore: registered new interface driver hub
[ 0.181429] usbcore: registered new device driver usb
[ 0.182250] omap_i2c 4802a000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c1_pins, deferring probe
[ 0.182274] platform 4802a000.i2c: Driver omap_i2c requests probe deferral
[ 0.182468] media: Linux media interface: v0.10
[ 0.182610] Linux video capture interface: v2.00
[ 0.182816] pps_core: LinuxPPS API ver. 1 registered
[ 0.182823] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.182928] PTP clock support registered
[ 0.185076] Switched to clocksource timer1
[ 0.200250] NET: Registered protocol family 2
[ 0.200867] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.200993] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.201061] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.201164] TCP: reno registered
[ 0.201177] UDP hash table entries: 512 (order: 1, 8192 bytes)
[ 0.201200] UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)
[ 0.201385] NET: Registered protocol family 1
[ 0.201770] RPC: Registered named UNIX socket transport module.
[ 0.201778] RPC: Registered udp transport module.
[ 0.201783] RPC: Registered tcp transport module.
[ 0.201790] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.202633] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.203215] PM: Loading am335x-pm-firmware.binbounce pool size: 64 pages
[ 0.323167] VFS: Disk quotas dquot_6.5.2
[ 0.323234] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.323811] NFS: Registering the id_resolver key type
[ 0.323893] Key type id_resolver registered
[ 0.323900] Key type id_legacy registered
[ 0.323937] jffs2: version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc.
[ 0.324116] msgmni has been set to 1485
[ 0.325538] NET: Registered protocol family 38
[ 0.325585] io scheduler noop registered
[ 0.325593] io scheduler deadline registered
[ 0.325614] io scheduler cfq registered (default)
[ 0.325631] Interrupt test module loaded
[ 0.325667] error
[ 0.327392] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.384775] Console: switching to colour frame buffer device 128x48
[ 0.394926] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.397566] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a OMAP UART0
[ 0.398354] 48022000.serial: ttyO1 at MMIO 0x48022000 (irq = 89, base_baud = 3000000) is a OMAP UART1
[ 1.186278] console [ttyO1] enabled
[ 1.190707] 48024000.serial: ttyO2 at MMIO 0x48024000 (irq = 90, base_baud = 3000000) is a OMAP UART2
[ 1.201736] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 1.217202] brd: module loaded
[ 1.224739] loop: module loaded
[ 1.228487] (stk) :sysfs entries created
[ 1.232650] (stk) : debugfs entries created
[ 1.239714] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.249644] usbcore: registered new interface driver asix
[ 1.255537] usbcore: registered new interface driver ax88179_178a
[ 1.262070] usbcore: registered new interface driver cdc_ether
[ 1.268315] usbcore: registered new interface driver r815x
[ 1.274222] usbcore: registered new interface driver smsc95xx
[ 1.280363] usbcore: registered new interface driver net1080
[ 1.286432] usbcore: registered new interface driver cdc_subset
[ 1.292766] usbcore: registered new interface driver zaurus
[ 1.298804] usbcore: registered new interface driver cdc_ncm
[ 1.305225] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.312067] ehci-pci: EHCI PCI platform driver
[ 1.316927] ehci-omap: OMAP-EHCI Host Controller driver
[ 1.323151] usbcore: registered new interface driver cdc_wdm
[ 1.329287] usbcore: registered new interface driver usb-storage
[ 1.336537] mousedev: PS/2 mouse device common for all mice
[ 1.343307] i2c-core: driver [NuTouch] using legacy suspend method
[ 1.349840] i2c-core: driver [NuTouch] using legacy resume method
[ 1.357960] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 1.366176] i2c /dev entries driver
[ 1.370310] Driver for 1-wire Dallas network protocol.
[ 1.377875] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.386756] edma-dma-engine edma-dma-engine.0: allocated channel for 0:25
[ 1.393914] edma-dma-engine edma-dma-engine.0: allocated channel for 0:24
[ 1.401217] omap_hsmmc 48060000.mmc: unable to get vmmc regulator -517
[ 1.408115] edma-dma-engine edma-dma-engine.0: freeing channel for 24
[ 1.414873] edma-dma-engine edma-dma-engine.0: freeing channel for 25
[ 1.421724] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral
[ 1.429350] edma-dma-engine edma-dma-engine.0: allocated channel for 0:13
[ 1.436504] edma-dma-engine edma-dma-engine.0: allocated channel for 0:12
[ 1.545982] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.555781] edma-dma-engine edma-dma-engine.0: allocated channel for 0:36
[ 1.563017] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 1.570344] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 1.576563] edma-dma-engine edma-dma-engine.0: allocated channel for 0:5
[ 1.583652] edma-dma-engine edma-dma-engine.0: allocated channel for 0:6
[ 1.593192] usbcore: registered new interface driver usbhid
[ 1.599077] usbhid: USB HID core driver
[ 1.605190] oprofile: no performance counters
[ 1.610142] oprofile: using timer interrupt.
[ 1.614909] TCP: cubic registered
[ 1.618420] Initializing XFRM netlink socket
[ 1.622963] NET: Registered protocol family 17
[ 1.627687] NET: Registered protocol family 15
[ 1.632392] 8021q: 802.1Q VLAN Support v1.8
[ 1.636875] Key type dns_resolver registered
[ 1.641989] cpu cpu0: cpu0 regulator not ready, retry
[ 1.647429] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
[ 1.655728] ThumbEE CPU extension supported.
[ 1.662153] omap_i2c 4802a000.i2c: did not get pins for i2c error: -19
[ 1.670634] tps65910 1-002d: No interrupt support, no core IRQ
[ 1.678754] vrtc: 1800 mV
[ 1.681844] vrtc: supplied by vbat
[ 1.686739] vio: at 1500 mV
[ 1.689822] vio: supplied by vbat
[ 1.694569] vdd_mpu: 912 <--> 1375 mV at 1325 mV
[ 1.699575] vdd_mpu: supplied by vbat
[ 1.704695] vdd_core: 912 <--> 1150 mV at 1137 mV
[ 1.709783] vdd_core: supplied by vbat
[ 1.714775] vdd3: 5000 mV
[ 1.718685] vdig1: at 1800 mV
[ 1.721941] vdig1: supplied by vbat
[ 1.726714] vdig2: at 1800 mV
[ 1.729969] vdig2: supplied by vbat
[ 1.734707] vpll: at 1800 mV
[ 1.737887] vpll: supplied by vbat
[ 1.742542] vdac: at 1800 mV
[ 1.745718] vdac: supplied by vbat
[ 1.750396] vaux1: at 1800 mV
[ 1.753642] vaux1: supplied by vbat
[ 1.758390] vaux2: at 3300 mV
[ 1.761634] vaux2: supplied by vbat
[ 1.766407] vaux33: at 3300 mV
[ 1.769752] vaux33: supplied by vbat
[ 1.774584] vmmc: 1800 <--> 3300 mV at 3300 mV
[ 1.779456] vmmc: supplied by vbat
[ 1.784336] NuTouch: nutouch_probe
[ 1.788130] Auto Tune Enabled ...
[ 1.791782] NuTouch: NUTOUCH_AutoTune
[ 1.796170] input: nutouch as /devices/virtual/input/input0
[ 1.802648] NUTOUCH_SyncWithThreadToReadMsg, boot is 1
[ 1.808078] NuTouch: boot request_irq
[ 1.812156] ------------[ cut here ]------------
[ 1.817029] WARNING: CPU: 0 PID: 9 at kernel/irq/manage.c:437 __enable_irq+0x3c/0xe0()
[ 1.825322] Unbalanced enable for IRQ 172
[ 1.829518] Modules linked in:
[ 1.832727] CPU: 0 PID: 9 Comm: kworker/u2:1 Tainted: G W 3.12.10-ti2013.12.01 #38
[ 1.841591] Workqueue: deferwq deferred_probe_work_func
[ 1.847064] Backtrace:
[ 1.849637] [<c0017880>] (dump_backtrace+0x0/0x10c) from [<c0017a1c>] (show_stack+0x18/0x1c)
[ 1.858476] r6:c0072290 r5:00000009 r4:ed0b9b28 r3:c07fd37c
[ 1.864432] [<c0017a04>] (show_stack+0x0/0x1c) from [<c056de50>] (dump_stack+0x20/0x28)
[ 1.872828] [<c056de30>] (dump_stack+0x0/0x28) from [<c0046d08>] (warn_slowpath_common+0x70/0x90)
[ 1.882130] [<c0046c98>] (warn_slowpath_common+0x0/0x90) from [<c0046dcc>] (warn_slowpath_fmt+0x38/0x40)
[ 1.892061] r8:c084c36c r7:c081f0d0 r6:c08655d8 r5:000000ac r4:ed0b0540
[ 1.899103] [<c0046d94>] (warn_slowpath_fmt+0x0/0x40) from [<c0072290>] (__enable_irq+0x3c/0xe0)
[ 1.908306] r3:000000ac r2:c06ac374
[ 1.912058] [<c0072254>] (__enable_irq+0x0/0xe0) from [<c0072378>] (enable_irq+0x44/0x7c)
[ 1.920622] r4:ed0b0540
[ 1.923285] [<c0072334>] (enable_irq+0x0/0x7c) from [<c0430308>] (sps_ts_probe+0x3dc/0x764)
[ 1.932033] r5:ed2b6c88 r4:ed2b3000
[ 1.935787] [<c042ff2c>] (sps_ts_probe+0x0/0x764) from [<c043ac68>] (i2c_device_probe+0x80/0xc0)
[ 1.944997] [<c043abe8>] (i2c_device_probe+0x0/0xc0) from [<c0331940>] (driver_probe_device+0x104/0x240)
[ 1.954927] r6:00000000 r5:ed300620 r4:c0862c54 r3:c043abe8
[ 1.960873] [<c033183c>] (driver_probe_device+0x0/0x240) from [<c0331b5c>] (__device_attach+0x48/0x4c)
[ 1.970621] r7:ed2b3478 r6:c0331b14 r5:ed300620 r4:c081f0f8
[ 1.976567] [<c0331b14>] (__device_attach+0x0/0x4c) from [<c032fe1c>] (bus_for_each_drv+0x4c/0x94)
[ 1.985951] r5:ed300620 r4:00000000
[ 1.989705] [<c032fdd0>] (bus_for_each_drv+0x0/0x94) from [<c03317f8>] (device_attach+0x78/0x90)
[ 1.998908] r6:c081f9d4 r5:ed300654 r4:ed300620
[ 2.003758] [<c0331780>] (device_attach+0x0/0x90) from [<c0330d70>] (bus_probe_device+0x8c/0xb4)
[ 2.012959] r6:c081f9d4 r5:ed300620 r4:ed300620 r3:ed0a20c0
[ 2.018905] [<c0330ce4>] (bus_probe_device+0x0/0xb4) from [<c032ef08>] (device_add+0x34c/0x624)
[ 2.028015] r6:ed300628 r5:00000000 r4:ed300620 r3:fffffffe
[ 2.033961] [<c032ebbc>] (device_add+0x0/0x624) from [<c032f1fc>] (device_register+0x1c/0x20)
[ 2.042899] [<c032f1e0>] (device_register+0x0/0x20) from [<c043c3f8>] (i2c_new_device+0x140/0x180)
[ 2.052284] r4:ed300600 r3:ed2fd1c0
[ 2.056037] [<c043c2b8>] (i2c_new_device+0x0/0x180) from [<c043c914>] (i2c_register_adapter+0x27c/0x48c)
[ 2.065967] r8:ed2b3478 r7:ed0b9d30 r6:c1073a90 r5:ed2b3450 r4:00000000
[ 2.073008] [<c043c698>] (i2c_register_adapter+0x0/0x48c) from [<c043cb78>] (__i2c_add_numbered_adapter+0x54/0x78)
[ 2.083857] [<c043cb24>] (__i2c_add_numbered_adapter+0x0/0x78) from [<c043cc30>] (i2c_add_adapter+0x94/0xac)
[ 2.094152] r5:ed0c0610 r4:ed2b3450
[ 2.097904] [<c043cb9c>] (i2c_add_adapter+0x0/0xac) from [<c043cc6c>] (i2c_add_numbered_adapter+0x24/0x28)
[ 2.108017] r5:ed0c0610 r4:ed2b3410
[ 2.111772] [<c043cc48>] (i2c_add_numbered_adapter+0x0/0x28) from [<c043e378>] (omap_i2c_probe+0x4dc/0x73c)
[ 2.121984] [<c043de9c>] (omap_i2c_probe+0x0/0x73c) from [<c0332c74>] (platform_drv_probe+0x20/0x24)
[ 2.131557] [<c0332c54>] (platform_drv_probe+0x0/0x24) from [<c0331940>] (driver_probe_device+0x104/0x240)
[ 2.141679] [<c033183c>] (driver_probe_device+0x0/0x240) from [<c0331b5c>] (__device_attach+0x48/0x4c)
[ 2.151428] r7:ed074700 r6:c0331b14 r5:ed0c0610 r4:c081fb60
[ 2.157374] [<c0331b14>] (__device_attach+0x0/0x4c) from [<c032fe1c>] (bus_for_each_drv+0x4c/0x94)
[ 2.166759] r5:ed0c0610 r4:00000000
[ 2.170513] [<c032fdd0>] (bus_for_each_drv+0x0/0x94) from [<c03317f8>] (device_attach+0x78/0x90)
[ 2.179717] r6:c08118f0 r5:ed0c0644 r4:ed0c0610
[ 2.184567] [<c0331780>] (device_attach+0x0/0x90) from [<c0330d70>] (bus_probe_device+0x8c/0xb4)
[ 2.193769] r6:c08118f0 r5:ed0c0610 r4:ed0c0610 r3:ed069d40
[ 2.199716] [<c0330ce4>] (bus_probe_device+0x0/0xb4) from [<c033125c>] (deferred_probe_work_func+0x68/0x94)
[ 2.209919] r6:c0811890 r5:c081189c r4:ed0c0610 r3:c0811e90
[ 2.215872] [<c03311f4>] (deferred_probe_work_func+0x0/0x94) from [<c0059f50>] (process_one_work+0xfc/0x340)
[ 2.226166] r6:ed06b800 r5:c08118b4 r4:ed09e3c0 r3:c03311f4
[ 2.232113] [<c0059e54>] (process_one_work+0x0/0x340) from [<c005a558>] (worker_thread+0x130/0x370)
[ 2.241598] [<c005a428>] (worker_thread+0x0/0x370) from [<c005fbdc>] (kthread+0xac/0xb8)
[ 2.250090] [<c005fb30>] (kthread+0x0/0xb8) from [<c00146f8>] (ret_from_fork+0x14/0x3c)
[ 2.258473] r7:00000000 r6:00000000 r5:c005fb30 r4:ed095e74
[ 2.264415] ---[ end trace 1b75b31a2719ed1e ]---
[ 2.269557] NuTouch: register chrdev(246,0)
[ 2.274664] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
[ 2.281498] edma-dma-engine edma-dma-engine.0: allocated channel for 0:25
[ 2.288695] edma-dma-engine edma-dma-engine.0: allocated channel for 0:24
[ 2.382604] mmc1: host does not support reading read-only switch. assuming write-enable.
[ 2.393609] mmc1: new high speed SDHC card at address 1234
[ 2.399395] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 2.405795] davinci_mdio 4a101000.mdio: detected phy mask ffffff7f
[ 2.412892] mmcblk0: mmc1:1234 SA04G 3.63 GiB
[ 2.419155] libphy: 4a101000.mdio: probed
[ 2.423417] davinci_mdio 4a101000.mdio: phy[7]: device 4a101000.mdio:07, driver unknown
[ 2.431997] mmcblk0: p1 p2
[ 2.436547] Detected MACID = 1c:ba:8c:e1:51:56
[ 2.443520] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 2.460370] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
[ 2.468119] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
[ 11.658527] EXT4-fs (mmcblk0p2): recovery complete
[ 12.327407] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 12.335996] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[ 12.347861] devtmpfs: mounted
[ 12.351642] Freeing unused kernel memory: 344K (c0750000 - c07a6000)
INIT: version 2.88 booting
Starting udev
[ 13.099396] udevd[816]: starting version 182
[ 13.371353] Bluetooth: Core ver 2.16
[ 13.432319] NET: Registered protocol family 31
[ 13.437107] Bluetooth: HCI device and connection manager initialized
[ 13.571230] Bluetooth: HCI socket layer initialized
[ 13.603115] PM: CM3 Firmware Version = 0x186
[ 13.643178] Bluetooth: L2CAP socket layer initialized
[ 13.713547] Bluetooth: SCO socket layer initialized
[ 13.805288] (stc): chnl_id list empty :4
[ 13.809409] (stk) : st_kim_start(stk) :ldisc_install = 1
[ 14.935259] (stk) :ldisc installation timeout(stk) :ldisc_install = 0
[ 15.935218] (stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1[ 16.581178] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Pl.
[ 16.788693] cryptodev: driver 1.6 loaded.
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
[ 16.880328] EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered

[ 17.045190] (stk) :ldisc installation timeout(stk) :ldisc_install = 0ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1696: No soundcards found...
Configuring network interfaces... [ 17.654080] net eth0: initializing cpsw version 1.12 (0)
[ 17.661367] libphy: PHY 4a101000.mdio:00 not found
[ 17.666415] net eth0: phy 4a101000.mdio:00 not found on slave 0
[ 17.672925] net eth0: phy found : id is : 0x221622
[ 17.685792] 8021q: adding VLAN 0 to HW filter on device eth0
udhcpc (v1.20.2) started
Sending discover...

[ 18.045170] (stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1
[ 19.155151] (stk) :ldisc installation timeout(stk) :ldisc_install = 0
[ 20.155156] (stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1Sending discover...

[ 21.265169] (stk) :ldisc installation timeout(stk) :ldisc_install = 0
[ 22.265168] (stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1
[ 23.375155] (stk) :ldisc installation timeout(stk) :ldisc_install = 0Sending discover...

[ 24.375164] (stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1
[ 25.485149] (stk) :ldisc installation timeout(stk) :ldisc_install = 0
[ 26.485147] (stk) : timed out waiting for ldisc to be un-installed[ 26.493630] Bluetooth: st_register failed -22
No lease, failing
done.
Mon Mar 31 02:34:00 UTC 2014
INIT: Entering runlevel: 5
Starting system message bus: dbus.
UIM SYSFS Node Found at /sys/./devices/kim.7/install
Starting uim-sysfs daemon.
uim:@ main
uim:install = /sys/./devices/kim.7/install
uim:dev_name = /sys/./devices/kim.7/dev_name
uim:baud_rate = /sys/./devices/kim.7/baud_rate
uim:flow_cntrl = /sys/./devices/kim.7/flow_cntrl
uim:begin polling...
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
Starting Lighttpd Web Server: lighttpd.
2000-01-01 00:00:00: (log.c.166) server started
Calibrating touchscreen (first time only)Couldnt open tslib config file: No such file or directory
ts_config: No such file or directory
.
/
Starting Matrix GUI application.
ERROR: could not insert 'g_mass_storage': No such device
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
binutils-symlinks
binutils
gdbserver

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.

_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|

Arago Project http://arago-project.org am335x-evm ttyO1

Arago 2013.12 am335x-evm ttyO1

am335x-evm login: root
root@am335x-evm:~# cd /home/root/ss1/
root@am335x-evm:~/ss1# ./SS1BTPM &
[1] 1440
root@am335x-evm:~/ss1# ./LinuxSPPM

******************************************************************
* Command Options: 1) Initialize *
* 2) Cleanup *
* 3) QueryDebugZoneMask *
* 4) SetDebugZoneMask *
* 5) ShutdownService *
* 6) RegisterEventCallback, *
* 7) UnRegisterEventCallback, *
* 8) QueryDevicePower *
* 9) SetDevicePower *
* 10)QueryLocalDeviceProperties *
* 11)SetLocalDeviceName *
* 12)SetLocalClassOfDevice *
* 13)SetDiscoverable *
* 14)SetConnectable *
* 15)SetPairable *
* 16)StartDeviceDiscovery *
* 17)StopDeviceDiscovery *
* 18)QueryRemoteDeviceList *
* 19)QueryRemoteDeviceProperties *
* 20)AddRemoteDevice *
* 21)DeleteRemoteDevice *
* 22)PairWithRemoteDevice *
* 23)CancelPairWithRemoteDevice *
* 24)UnPairRemoteDevice *
* 25)QueryRemoteDeviceServices *
* 26)RegisterAuthentication *
* 27)UnRegisterAuthentication *
* 28)PINCodeResponse *
* 29)PassKeyResponse *
* 30)UserConfirmationResponse *
* 31)ChangeSimplePairingParameters *
* 32)RegisterServerPort *
* 33)OpenServerPortRequestResponse *
* 34)UnRegisterServerPort *
* 35)OpenRemotePort *
* 36)ClosePort *
* 37)ReadData *
* 38)WriteData *
* 39)SendLineStatus *
* 40)SendPortStatus *
* 41)QueryServerPresent *
* 42)FindFreeServerPort *
* 43)ChangeBufferSize *
* 44)LoopbackMode *
* 45)AutomaticReadMode *
* 46)DisplayRawDataMode *
* Help, Quit. *
******************************************************************
SPPM>1 1'^H

BTPM_Initialize() Success: 0.
DEVM_RegisterEventCallback() Success: 5.
SPPM> ^H

Invalid Command.
SPPM>9

Usage: SetDevicePower [0/1 - Power Off/Power On].
Function Error.
SPPM>9 1

DEVM_PowerOnDevice() Failure: -14, Unknown Error.
Function Error.
SPPM>


Regards,
Balaji

dts+log.zip
  • Hi,

    The error you are facing is “BTPS_ERROR_HCI_DRIVER_ERROR(-14)”. usually we see this only when we have some UART interface problem. Please make sure your uart configuration is fine.

    From the software point below are the steps you need to follow for bringing up Am335x+WL18xx:

    Please see http://processors.wiki.ti.com/index.php?title=WL18xx_AMxxx_platform_integration_guide 

    Get the am335x-evm-sdk-src-07.00.00.00.tar.gz and am335x-evm-sdk-bin-07.00.00.00.tar.gz fromhttp://software-dl.ti.com/sitara_linux/esd/AM335xSDK/latest/index_FDS.html, link to this is provided in the previous link.

    extract the src and applied the patches and built with the Cross compiler (arm-linux-gnueabihf-), you can get the cross compiler from the above link or even if you install the "install.bin", you will have it at location "ti-sdk-am335x-evm-07.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/"

    and once the kernel is built you can copy the .dtb and ZImage to the boot partition. after extracting the bin folder, You will see the file system directly which you can copy to ROOTFS (file-system) partition. UIM is already part of this file-system.

    Install the Bluetopia SDK on your PC, and just copy the executables from "BluetopiaPM/bin" of your PC to "/home/root/ss1" of the file-system.

  • Hi

    Thanks for the immediate response. I've reviewed the changes for our hardware again with the dts file and could not find any obvious issues in pin mapping.

    Can you please let me know how to debug and find if it is a UART configuration issue? We are able to see tty02 being created successfully and when we tried sending/receiving through tty2 using microcosm utility we are able to see transactions using CRO.

    Would be of help if you can let me know if there are any debug mechanisms to find further inputs

    Balaji

  • Hi Sundeep,
    We checked our dts file again and now we've got the below error when we typed SetDevicePower command.

    Can you please let me know what could be the root cause of this error?

    SPPM>1 1

    BTPM_Initialize() Success: 0.
    DEVM_RegisterEventCallback() Success: 5.
    SPPM>9 1

    [ 65.541767] (hci_tty): inside hci_tty_open (ed27a358, ed0a3e00)
    [ 65.548103] (stc): chnl_id list empty :4
    [ 65.552218] (stk) : st_kim_start(stk) :ldisc_install = 1uim:poll broke due to event 10()

    uim:read 1 f
    [ 65.664414] (stc): st_tty_open rom install

    uim:@ st_uart_config
    uim: signa(stk) :line discipline installedl received, opening /dev/ttyO2
    uim:@ set_baud_rate
    uim:set_bau
    [ 65.681252] (stk) :TIInit_11.8.32.btsd_rate() done
    uim:Installed N_TI_WL Line displine
    uim:begin polling...
    (stk) :change remote baud rate command in firmware
    [ 65.706367] (stk) :skipping the wait event of change remote baud(stk) :sleep command inr
    [ 68.151146] (stk) :sleep command in scr[ 71.922726] (stc): add_channel_to_table: id 4
    [ 71.927346] (stc): add_channel_to_table: id 2
    [ 71.931916] (stc): add_channel_to_table: id 3
    [ 71.963240] (hci_tty): inside hci_tty_release (ed27a358, ed0a3e00)
    [ 71.969746] (stc): remove_channel_from_table: id 4
    [ 71.974798] (stc): remove_channel_from_table: id 2
    [ 71.979826] (stc): remove_channel_from_table: id 3
    [ 71.984857] (stc): all chnl_ids unregistered
    [ 71.989344] (stk) :ldisc_install = 0uim:poll broke due to event 10(PRI:2/ERR:8)(stc): s

    uim:read 0 from install

    uim:@ st_uart_config
    uim:Un-Installed N_TI_WL Line displine
    uim:begin polling...
    DEVM_PowerOnDevice() Failure: -3, Unknown Error.
    Function Error.

    Regards,
    Balaji

  • Hi,

    You are getting BTPS_ERROR_STACK_INITIALIZATION_ERROR that is strange.

    I hope it might be related to the system clock (saw a similar issue before).

    Could you please set the clock (date) to the current time and rebuild your code and see if it helps.

  • hi Sundeep,
    One update in the exercise. We tried using  hcitool to check if the low level interface is working. It looks like hcitool is working fine whereas the problem happens only when we try using Bluetopia stack.

    Please let us know why the stack behaves differently during the same sequence as HCItool. I've highlighted in yellow for quick reference.


    Below are the logs:

    root@am335x-evm:~/ss1# ./SS1BTPM &
    [1] 1377
    root@am335x-evm:~/ss1# ./LinuxSPPM

    ******************************************************************
    * Command Options: 1) Initialize *
    * 2) Cleanup *
    * 3) QueryDebugZoneMask *
    * 4) SetDebugZoneMask *
    * 5) ShutdownService *
    * 6) RegisterEventCallback, *
    * 7) UnRegisterEventCallback, *
    * 8) QueryDevicePower *
    * 9) SetDevicePower *
    * 10)QueryLocalDeviceProperties *
    * 11)SetLocalDeviceName *
    * 12)SetLocalClassOfDevice *
    * 13)SetDiscoverable *
    * 14)SetConnectable *
    * 15)SetPairable *
    * 16)StartDeviceDiscovery *
    * 17)StopDeviceDiscovery *
    * 18)QueryRemoteDeviceList *
    * 19)QueryRemoteDeviceProperties *
    * 20)AddRemoteDevice *
    * 21)DeleteRemoteDevice *
    * 22)PairWithRemoteDevice *
    * 23)CancelPairWithRemoteDevice *
    * 24)UnPairRemoteDevice *
    * 25)QueryRemoteDeviceServices *
    * 26)RegisterAuthentication *
    * 27)UnRegisterAuthentication *
    * 28)PINCodeResponse *
    * 29)PassKeyResponse *
    * 30)UserConfirmationResponse *
    * 31)ChangeSimplePairingParameters *
    * 32)RegisterServerPort *
    * 33)OpenServerPortRequestResponse *
    * 34)UnRegisterServerPort *
    * 35)OpenRemotePort *
    * 36)ClosePort *
    * 37)ReadData *
    * 38)WriteData *
    * 39)SendLineStatus *
    * 40)SendPortStatus *
    * 41)QueryServerPresent *
    * 42)FindFreeServerPort *
    * 43)ChangeBufferSize *
    * 44)LoopbackMode *
    * 45)AutomaticReadMode *
    * 46)DisplayRawDataMode *
    * Help, Quit. *
    ******************************************************************
    SPPM>1 1

    BTPM_Initialize() Success: 0.
    DEVM_RegisterEventCallback() Success: 5.
    SPPM>9 1

    [ 68.119686] (hci_tty): inside hci_tty_open (ed27a358, ed5722c0)

    [ 68.126028] (stc): chnl_id list empty :4 (stk) : st_kim_start
    [ 68.236789] (stk) :ldisc_install = 1uim:poll broke due to event 10(PRI:2/ERR:8)(stc): st_tty_open

    uim:read 1 from install

    uim:@ st_uart_co
    [ 68.247193] (stk) :line discipline installednfig
    uim: signal received, opening /dev/ttyO2
    uim:@ set_baud_r(stk) :TIInit_11.8.32.btsate
    uim:set_baud_rate() done
    uim:Installed N_TI_WL Line displine
    uim:begin polling...

    [ 68.269632] (stk) :change remote baud rate command in firmware(stk) :skipping the wait event of change remote baud
    [ 70.217155] (stk) :sleep command in scr(stk) :sleep command in scr
    [ 74.490526] (stc): add_channel_to_table: id 4
    [ 74.495336] (stc): add_channel_to_table: id 2
    [ 74.499903] (stc): add_channel_to_table: id 3
    [ 74.531346] (hci_tty): inside hci_tty_release (ed27a358, ed5722c0)
    [ 74.537908] (stc): remove_channel_from_table: id 4
    [ 74.542949] (stc): remove_channel_from_table: id 2
    [ 74.547968] (stc): remove_channel_from_table: id 3
    [ 74.552997] (stc): all chnl_ids unregistered
    [ 74.557489] (stk) :ldisc_install = 0uim:poll broke due to event 10(PRI:2/ERR:8)(stc): st_tty_close

    uim:read 0 from install

    uim:@ st_uart_config
    uim:Un-Installed N_TI_WL Line displine
    uim:begin polling...
    DEVM_PowerOnDevice() Failure: -3, Unknown Error.
    Function Error.

    SPPM>quit

    root@am335x-evm:~/ss1# hciconfig -a
    hci0: Type: BR/EDR Bus: UART
    BD Address: 1C:BA:8C:84:18:6C ACL MTU: 1021:6 SCO MTU: 180:4
    DOWN
    RX bytes:547 acl:0 sco:0 events:27 errors:0
    TX bytes:411 acl:0 sco:0 commands:27 errors:0
    Features: 0xff 0xfe 0x2d 0xfe 0xdb 0xff 0x7b 0x87
    Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3
    Link policy: RSWITCH HOLD SNIFF
    Link mode: SLAVE ACCEPT

    root@am335x-evm:~/ss1# hciconfig hci0 up

    [ 105.197871] (stc): chnl_id list empty :4 (stk) : st_kim_start
    [ 105.308746] (stk) :ldisc_install = 1uim:poll broke due to event 10(PRI:2/ERR:8)(stc): st_tty_open

    uim:read 1 from install

    uim:@ st_uart_co
    [ 105.319679] (stk) :line discipline installednfig
    uim: signal received, opening /dev/ttyO2
    uim:@ set_baud_r(stk) :TIInit_11.8.32.btsate
    uim:set_baud_rate() done
    uim:Installed N_TI_WL Line displine
    uim:begin polling...

    [ 105.342225] (stk) :change remote baud rate command in firmware(stk) :skipping the wait event of change remote baud
    [ 107.289713] (stk) :sleep command in scr(stk) :sleep command in scr
    [ 111.562471] (stc): add_channel_to_table: id 4
    [ 111.567276] (stc): add_channel_to_table: id 2
    [ 111.571847] (stc): add_channel_to_table: id 3
    root@am335x-evm:~/ss1# hcitool scan
    Scanning ...
    3C:25:D7:60:73:D4 Windows Phone
    4C:A5:6D:AF:3B:B7 Galaxy S4
    60:A4:4C:98:65:88 Nexus 7
    root@am335x-evm:~/ss1#

  • Hi Sundeep,
    We tried re-building the kernel also without any luck. We enabled the verbose and debug messages in uim.c and i'm attaching the log we got. 

    Let me know if there is a problem with the stack usage/porting.

    SPPM>1 1

    BTPM_Initialize() Success: 0.
    DEVM_RegisterEventCallback() Success: 5.
    SPPM>9 1


    Changing Baudrate
    [ 68.083653] (hci_tty): inside hci_tty_open (ed27a358, ed0a35c0)

    [ 68.091172] (stc): chnl_id list empty :4 (stk) : st_kim_start
    [ 68.201961] (stk) :ldisc_install = 1uim:poll broke due to event 10(PRI:2/ERR:8)

    uim:read 1 from install

    uim:@ st_uart_config
    uim: signal received, opening /dev/ttyO2
    uim:@ set_baud_rate
    uim:set_baud_rate() done
    uim:Setting speed to 3000000
    uim:@ read_command_complete
    uim: Command complete started
    uim:@ read_hci_event
    uim: read_hci_event
    uim:Command complete done
    uim:Speed changi(stc): st_tty_open ng to 3000000, 1
    uim:@ set_custom_baud_rate

    [ 68.262713] (stk) :line discipline installeduim:Installed N_TI_WL Line displine(stk) :TIInit_11.8.32.bts
    uim:begin polling...

    [ 68.280023] (stk) :change remote baud rate command in firmware(stk) :skipping the wait event of change remote baud
    [ 68.473280] (stk) :sleep command in scr(stk) :sleep command in scr
    [ 69.918231] (stc): add_channel_to_table: id 4
    [ 69.923013] (stc): add_channel_to_table: id 2
    [ 69.927602] (stc): add_channel_to_table: id 3
    [ 69.936249] <out<01 03 0c 00
    [ 69.939611] >rx>0e 04 01 03 0c 00
    [ 69.943164] >in>0e 04 01 03 0c 00
    [ 69.947799] <out<01 01 10 00
    [ 69.951058] >rx>0e 0c 01 01 10 00 06 00 00 06 0d 00 70 ac
    [ 69.956801] >in>0e 0c 01 01 10 00 06 00 00 06 0d 00 70 ac
    [ 69.963432] <out<01 03 10 00
    [ 69.966668] >rx>0e 0c 01 03 10 00 ff fe 2d fe db ff 7b 87
    [ 69.972377] >in>0e 0c 01 03 10 00 ff fe 2d fe db ff 7b 87
    [ 69.979024] <out<01 01 0c 08 ff ff ff ff ff ff ff 3f
    [ 69.984547] >rx>0e 04 01 01 0c 00
    [ 69.988113] >in>0e 04 01 01 0c 00
    [ 69.991666] <out<01 6d 0c 02 01 00
    [ 69.995693] >rx>0e 04 01 6d 0c 00
    [ 69.999212] >in>0e 04 01 6d 0c 00
    [ 70.003747] <out<01 02 10 00
    [ 70.007189] >rx>0e 44 01 02 10 00 ff ff ff 03 ce ff ff ff 0f ff
    [ 70.013394] >rx>ff 1f f2 0f e8 fe 3f f7 8f ff 1c 00 00 00 61 f7
    [ 70.019598] >rx>ff ff 7f 38 00 00 00 00 00 00 00 00 00 00 00 00
    [ 70.025802] >rx>00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
    [ 70.032006] >rx>00 00 00 00 00 00
    [ 70.035551] >in>0e 44 01 02 10 00 ff ff ff 03 ce ff ff ff 0f ff
    [ 70.041760] >in>ff 1f f2 0f e8 fe 3f f7 8f ff 1c 00 00 00 61 f7
    [ 70.047990] >in>ff ff 7f 38 00 00 00 00 00 00 00 00 00 00 00 00
    [ 70.054206] >in>00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
    [ 70.060411] >in>00 00 00 00 00 00
    [ 70.065778] <out<01 01 10 00
    [ 70.069054] >rx>0e 0c 01 01 10 00 06 00 00 06 0d 00 70 ac
    [ 70.074811] >in>0e 0c 01 01 10 00 06 00 00 06 0d 00 70 ac
    [ 70.081546] <out<01 bc fd 00
    [ 70.084897] >rx>0e 05 01 bc fd 00 00
    [ 70.088769] >in>0e 05 01 bc fd 00 00
    [ 70.094031] <out<01 09 10 00
    [ 70.097295] >rx>0e 0a 01 09 10 00 6c 18 84 8c ba 1c
    [ 70.102579] >in>0e 0a 01 09 10 00 6c 18 84 8c ba 1c
    [ 70.110249] (hci_tty): inside hci_tty_release (ed27a358, ed0a35c0)
    [ 70.116794] (stc): remove_channel_from_table: id 4
    [ 70.121816] (stc): remove_channel_from_table: id 2
    [ 70.126854] (stc): remove_channel_from_table: id 3
    [ 70.131876] (stc): all chnl_ids unregistered
    [ 70.136374] (stk) :ldisc_install = 0uim:poll broke due to event 10(PRI:2/ERR:8)(stc): st_tty_close

    uim:read 0 from install

    uim:@ st_uart_config
    uim:Un-Installed N_TI_WL Line displine
    uim:begin polling...
    DEVM_PowerOnDevice() Failure: -3, Unknown Error.
    Function Error.
    SPPM>

    Regards,
    Balaji

  • Hi Sundeep,

    Thanks for the pointers. The BT stack is working now.

    We had our RTC connected through SPI interface and we never brought it up.  So we manually set the date and time using "date" command in Linux and then ran the stack and it started working.
    Strange that it has a dependency on RTC but it has kept us going.
    Thanks once again
    Regards,
    Balaji