Other Parts Discussed in Thread: CC3200, UNIFLASH, CC3200-LAUNCHXL
PROBLEM
- Unable to set CC3200.ccxml as default configuration file.
- Unable to launch CCS debug session because CCS cannot find CC3200.ccxml.
ENVIRONMENT
- Windows Vista
- All software is installed in C:\ti
- CCS ver 6.0.1.00040
- Uniflash ver 3.2.0.00065
- CC3200 SDK ver 1.0.0
- CC31xx/CC32xx Service Pack 1.0.0.1.1
- Board: CC3200-LAUNCHXL Rev 4.1
- Virus detection sofware is off
- Device manager shows "CC3200LP Dual Port (COM19)" under port devices
SYNOPSIS
I'm trying to run the wlan_station project as described by SWRU376A, "CC3200 SimpleLink Getting Started Guide." I've performed all the instructions as described by the guide.
When I arrived at Steps 13, 14, and 15, I imported a copy of CC3200.ccxml and failed to set it as the default target configuration. When I right-mouse button clicked on the file, and selected Set as Default, the command failed. The file name was suposed to become bolded and appended with the string [Default], as so: CC3200.ccxml [Default].
When I logged into the Windows administrator's account, started CCS, and imported the file, I was able to set it as default. But it didn't stick.
Now, back in my regular Windows account, when I attempted to build the project, it failed, and CCS presented this message.
"Unable to launch CCS debug-session based on current selection. The specified file "C:\ti\ccsv6\ti\CCSTargetConfigurations\CC3200.ccxml" does not exist in the file system."
This is true. There is no ...\ti\CCSTargetConfigurations\ directory, nor is there such a directory installed anywhere in C:\ti\ccsv6. I have resinstalled CCS and assured that the CC32xx device support package is installed, but with no affect.
It seems to me that there was an installation problem, but it wasn't corrected by performing another installation. Seems like both problems are related.