This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Adding button interface to out_of_the_box for cc3200 lunchpad does not compile

Dear All,

I am trying to add buttons to the a projec called Boiler which is the same as out_of_the_box example.

I have included button_if.h in main.c:

// Common interface includes
#include "gpio_if.h"
#include "uart_if.h"
#include "i2c_if.h"
#include "button_if.h" // 12.11.2014 IlanS - need to use buttons therefore we need this include
#include "common.h"

Also added the folloing functions:

void SystemONInterruptHandler()
{
GPIO_IF_LedOn(MCU_RED_LED_GPIO);
}
void SystemOFFInterruptHandler()
{
GPIO_IF_LedOff(MCU_RED_LED_GPIO);
}

and the following line in BoardInit function:

Button_IF_Init(SystemOFFInterruptHandler,SystemONInterruptHandler);

When trying to build the broject, I get the folloing errors:

#10010 errors encountered during linking; "Boiler.out" not built Boiler 

#10234-D</a> unresolved symbols remain Boiler 

Description Resource Path Location Typeunresolved symbol Button_IF_Init, first referenced in ./main.obj Boiler 

 

thanks

Ilan