I am just starting with the CC3200. I worked through the setup issues using the CC3200 Getting Started Guide. I set the jumpers per the picture in the Guide. I then installed SDK Service Pack 1.0.0.1.2 using Uniflash. I edited Common.h.
Using IAR 7.2, i installed the patch, recompiled SimpleLink, and then opened getting_started_with_wlan_station workspace.
This example connects to the AP fine. However, it fails on Pinging. I verified that both my gateway and and www.Ti.Com respond to pings from my computer over the same WiFi AP.
*************************************************
CC3200 WLAN STATION Application
*************************************************
Host Driver Version: 1.0.0.1
Build Version 2.2.7.1.31.1.2.4.2.1.5.3.23
Device is configured in default state
Device started as STATION
[WLAN EVENT] STA Connected to the AP: ISW4 ,BSSID: 0:e:3b:44:dd:b0
[NETAPP EVENT] IP Acquired: IP=192.168.111.185 , Gateway=192.168.111.1
Connection established w/ AP and IP is aquired
Pinging...!
Error [-2000] at line [667] in function [CheckLanConnection]
Device couldn't ping the gateway
I used ethernet trace to look for activity from the CC3200. I see QoS packets, but no ping packets.
I tried other examples of such as GetTime and GetWeather. They also seem to hang after opening a socket. These two examples fail on resolving DNS. They do not send any packets that make it to the gateway.
I am concerned that I have a configuration management issue. The teraterm information from above seems to indicate that I got the service pack installed correctly. I
Any ideas?