I made a test board based on the CC3200.
And I was sure that the power (VDD_DIG and VDD_ANA) and clock out well.
Also, I was link to CC3200 by CCS.
However, when I try to format the disk by Uniflash(Version: 3.2.0.00065), It failed likes following console script.
[22:20:32] INFO: --- please restart the device ---
[22:20:50] ERROR: ---reading ACK signal failed---
[22:20:50] FATAL: --- Can't connect to device !! ---
[22:30:40] FATAL: Error connecting to the device. Please check your COM port settings. Error code: -3
I think that well-connected to M25PX80 and Serial Comport.
Of course, I was also well connected SOP2 to pull-up(270 ohm).
And I tried plugging the comfort test on launch pad.
What I missed that before formatting the M25PX80?
In order to help you, I attach the schematic.5241.CC3200_test.pdf