Hi
I have IAR workbench 6.5 and I have a hard time to connect to CC3200 lunch pad to download and debugging code either my code or example codes.
I followed CC3200 programmer's guide for set up IAR project and I got this error
Tue Nov 18, 2014 08:40:50: JTAG Speed is set to: 500 kHz
Tue Nov 18, 2014 08:11:37: Fatal error: **ERROR**: JTAG initialization failed 0x00000004 Session aborted!
once start downloading session.
the fact is, IAR recognizes there is connection because when I unplug the board the error is different.
Tue Nov 18, 2014 08:40:25: Fatal error: **ERROR**: Unable to open device 0x00000002 Session aborted!
I have also reviewed other posts regarding this issue. Apparently, that problem never resolved. so I am hoping this post not only can solve my issue but also would be helpful for other developers.