Per the CC3100 docs, the new CC3100 has an option that allows it to be used with other MCUs, using
an adapter board called MCU-Adapt. Any idea on when more information about MCU-Adapt will be
available, and when the board will be coming out ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Leo,
CC3100 provides SPI and UART interface to connect to Host MCU. CC3100 BP has all lines routed on 20x020 header and can be blue wired to connect with any MCU EVMs.
On MCU-Adapt board, it is work in progress and will share the details as n when it is ready. However I hope it will not block you to use CC3100 with other MCU evm.
Regards,
Geet