Hi
we are designing a board with CC3100mod
We need info about some PIN
pin 39 VDD_ANA2- Power supply for CC3100 internal flash.
is it possible feed the internal Flash to VCC (in our case 3 volts) or do I have to use a 3.3V?
For the programming interface of the Serial Flash via CCS UniFlash
is it enough to have in a connector these pins
PIN 44 UART1_RTS
PIN 46 UART1_TX
PIN 47 UART1_RX
PIN 51 UART1_CTS
Is it the right interface?
best regards
Umberto S.