We've just just purchased a cc3200 launchpad from the TI web shop.
When it arrived, I installed the newest Code Composer, service packs, uniflash, flashed it, followed the start guides and so on. It seemed to work. Sort of. (There were some unexplained quirks here and there)
I wasn't able to make it connect to our WiFi WPA2 AP though. And it wasn't able to scan either. So I decided to set up an OPEN AP, placed on my desk, right next to the launchpad. Just to see it working.
Two day later I've set up the AP. (Distance: 1 m) But now I'm not able to run the sample code in Code Composer.
I'm able to compile, start up the debugger, step through the code, the LEDs are working, but whenever I get to a "sl_Start", the debugger fails with the following msg:
"Cortex_M4_0: Error: Connection with the target was unexpectedly lost."
I've tried several of the included projects. Same error. I've verified the jumpers. I've rebuild the projects, repowered everything, changing usb slot and so on.
I'm guessing that the unit is faulty and has been so on arrival? (Please correct me if I'm wrong.)
How and where do I contact TI, to send me a replacement?