i am developming a 6LowPan device using TI CC1120DK and would like to add WiFi to one of my 6LowPan nodes(the device is using MSP430F5438A as host MCU)
Is it possible to connect a CC3100BOOST to the CC1120DK? or are there another way to start developing with a MSP430F5438 MCU and a CC3100 WiFi chip?
I am aware that the CC1120DK doesn't have any 40-pin boosterpack slot, but I was thinking if it is possible to connect all pins that is utilized by the CC3100BOOST to the CC1120DK I/0 breakout pins (userguide page p24-25)