This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Clarification for Smart Plug with Remote Disconnect and Wi-Fi Connectivity design

Other Parts Discussed in Thread: CC3100, CC3200

Hi,

We are working on one of your project Smart Plug with Remote Disconnect and Wi-Fi Connectivity.

In the block diagram and in other specifications CC3200 is mentioned but  in the eagle files CC31xx is used which I feel is CC3100 family ( a  Wi-Fi Network Processor) whereas CC3200 is WiFI+MCU.

 Is the same design for smart plug with CC3200 is available even if the energy metering is not there it will be fine for now.

 Also need clarification that if I use CC31xx and later use CC3200 the programming part will be the same or we need to use different codes for that.

Currently I am working on CC3200 launchpad and got the .brd file but not  the .sch file  for the launchpad.