Hello!
one part of the expiriment that i want to conduct is the propogation of information from one cc3100 to other cc3100 units which are stations at the same network.
i woulkd like to understand the following things:
1. doesthe CC3100 has the ability to broadcast / multicast information as a member of a LAN?
2. if the anwser is "yes" what are the limitations of such broadcast?
3. if the anwser is "no" what are my alternetives?
thanx alot!