Hi,
It will be OK if I just enable only Wifi but when I enabled Bluetooth, I got that message:
root@OpenWrt:/# udhcpc -i wlan0 udhcpc (v1.22.1) started Sending discover... [ 56.999291] wlcore: ERROR SW watchdog interrupt received! starting recovery. [ 57.006711] ------------[ cut here ]------------ [ 57.011652] WARNING: CPU: 0 PID: 901 at drivers/net/wireless/ti/wlcore/main.c:801 wl1271_op_add_interface+0x88c/0x8c0 [wlcore]() [ 57.023806] Modules linked in: btwilink bluetooth 6lowpan_iphc pppoe ppp_async iptable_nat wl18xx pppox ppp_generic nf_nat_ipv4 nf_conntrack_ipv6 nf_conntrack_ipv4 krng ipt_MASQUERADE chainiv xt_time xt_tcpudp xt_state xt_nat xt_multiport xt_mark xt_mac xt_limit xt_id xt_conntrack xt_comment xt_TCPMSS xt_REDIRECT xt_LOG xt_CT wlcore_sdio wlcore slhc rng nf_nat_irc nf_nat_ftp nf_nat nf_defrag_ipv6 nf_defrag_ipv4 nf_conntrack_irc nf_conntrack_ftp nf_conntrack mac80211 iptable_raw iptable_mangle iptable_filter ipt_REJECT ip_tables ctr crypto_wq crc_itu_t crc_ccitt cfg80211 ccm aead ip6t_REJECT ip6table_raw ip6table_mangle ip6table_filter ip6_tables x_tables ipv6 arc4 crypto_blkcipher usbcore usb_common [ 57.089247] CPU: 0 PID: 901 Comm: irq/171-wl18xx Not tainted 3.14.18 #1 [ 57.096183] Backtrace: [ 57.098794] [<c001bea0>] (dump_backtrace) from [<c001c184>] (show_stack+0x18/0x1c) [ 57.106732] r6:bf196480 r5:00000000 r4:c053ad80 r3:00000000 [ 57.112721] [<c001c16c>] (show_stack) from [<c01aab5c>] (dump_stack+0x88/0x98) [ 57.120319] [<c01aaad4>] (dump_stack) from [<c0040ad4>] (warn_slowpath_common+0x78/0x94) [ 57.128819] r5:00000009 r4:00000000 [ 57.132581] [<c0040a5c>] (warn_slowpath_common) from [<c0040b94>] (warn_slowpath_null+0x24/0x2c) [ 57.141809] r8:df5496d8 r7:df549538 r6:df549550 r5:df549520 r4:df549500 [ 57.148893] [<c0040b70>] (warn_slowpath_null) from [<bf196480>] (wl1271_op_add_interface+0x88c/0x8c0 [wlcore]) [ 57.159421] [<bf196454>] (wl1271_op_add_interface [wlcore]) from [<bf1966d0>] (wlcore_irq+0xf8/0x540 [wlcore]) [ 57.169926] r4:df549500 r3:00000002 [ 57.173705] [<bf1965d8>] (wlcore_irq [wlcore]) from [<c007cfdc>] (irq_thread_fn+0x24/0x48) [ 57.182387] r9:df55df80 r8:df0e4540 r7:00000001 r6:00000000 r5:df0e4540 r4:df55df80 [ 57.190556] [<c007cfb8>] (irq_thread_fn) from [<c007d2bc>] (irq_thread+0xd0/0x17c) [ 57.198515] r6:00000000 r5:df430000 r4:df55dfa0 r3:00000004 [ 57.204484] [<c007d1ec>] (irq_thread) from [<c005c3c0>] (kthread+0xf0/0xf4) [ 57.211798] r10:00000000 r9:00000000 r8:00000000 r7:c007d1ec r6:df55df80 r5:00000000 [ 57.220050] r4:df55df40 [ 57.222716] [<c005c2d0>] (kthread) from [<c0008e58>] (ret_from_fork+0x14/0x3c) [ 57.230303] r7:00000000 r6:00000000 r5:c005c2d0 r4:df55df40 [ 57.236257] ---[ end trace 47bca053c8fa5fa8 ]--- [ 57.242237] wlcore: Hardware recovery in progress. FW ver: Rev 8.9.0.0.17 [ 57.249915] wlcore: pc: 0x12798, hint_sts: 0x00000000 count: 1 [ 57.256272] wlcore: down [ 57.260201] ieee80211 phy0: Hardware restart was requested [ 57.683940] wlcore: PHY firmware version: Rev 8.2.0.0.212 [ 57.780347] wlcore: firmware booted (Rev 8.9.0.0.17) [ 57.802928] wlcore: Association completed. Sending discover... Sending select for 192.168.168.117... Lease of 192.168.168.117 obtained, lease time 604800 udhcpc: ifconfig wlan0 192.168.168.117 netmask 255.255.255.0 broadcast 192.168.168.255 udhcpc: setting default routers: 192.168.168.1
My kernel is 3.14.8, and I tried to patch the "compat-wireless" (R8.4 release) to my kernel, maybe I missed or wrong in somewhere.
Thanks
Tuan Nguyen