Hi,
I am getting the following error while applying patch in yocto environment. Please explain what is this error about.
############################################################################################
patching file imx/meta-fsl-arm/recipes-kernel/linux/linux-imx-3.10.17/0001-Add-DT-support-for-wilink-8.patch
patching file imx/meta-fsl-arm/recipes-kernel/linux/linux-imx-3.10.17/0002-Patching-the-imx_v7_defconfig-for-Wilink-8-support.patch
can't find file to patch at input line 209
Perhaps you used the wrong -p or --strip option?
The text leading up to this was:
--------------------------
|diff --git a/imx/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb b/imx/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb
|index 422a54b..ac5e3ff 100644
|--- a/imx/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb
|+++ b/imx/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb
--------------------------
File to patch:
#####################################################################################################