This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WiLink8 R8.5 throughput problem

Other Parts Discussed in Thread: WL1835MOD

 I am trying to evaluate throughput of wl1835mod with beaglebone black. I am using pre-built images released by TI.

The module is set as host AP  and client is connected to AP. From my observation, what I am seeing is after sometime through of the module decreases and stays around the bandwidth. Does any one has seen this issue?

Here is my log:

[ 4388.132975] wlcore: PHY firmware version: Rev 8.2.0.0.224
[ 4388.298982] wlcore: firmware booted (Rev 8.9.0.0.31)
root@am335x-evm:~# wlan1: STA 78:dd:08:c6:f4:0a IEEE 802.11: authenticated
wlan1: STA 78:dd:08:c6:f4:0a IEEE 802.11: associated (aid 1)
wlan1: AP-STA-CONNECTED 78:dd:08:c6:f4:0a

root@am335x-evm:~#
root@am335x-evm:~# iperf -s
------------------------------------------------------------
Server listening on TCP port 5001
TCP window size: 85.3 KByte (default)
------------------------------------------------------------
[  4] local 10.4.30.34 port 5001 connected with 10.4.30.35 port 45192
[ ID] Interval       Transfer     Bandwidth
[  4]  0.0- 0.3 sec  1.00 MBytes  24.2 Mbits/sec
[  5] local 10.4.30.34 port 5001 connected with 10.4.30.35 port 45193
[  5]  0.0-28.3 sec   100 MBytes  29.7 Mbits/sec
[  4] local 10.4.30.34 port 5001 connected with 10.4.30.35 port 45194
[  4]  0.0-424.0 sec  1000 MBytes  19.8 Mbits/sec
[  5] local 10.4.30.34 port 5001 connected with 10.4.30.35 port 45195
[  5]  0.0-394.3 sec  1000 MBytes  21.3 Mbits/sec
[  4] local 10.4.30.34 port 5001 connected with 10.4.30.35 port 45196
[  4]  0.0-112.9 sec  3.25 MBytes   242 Kbits/sec
[  5] local 10.4.30.34 port 5001 connected with 10.4.30.35 port 45197
[  5]  0.0-275.9 sec  11.4 MBytes   346 Kbits/sec
[  4] local 10.4.30.34 port 5001 connected with 10.4.30.35 port 45198
[  4]  0.0-22.7 sec  1.00 MBytes   369 Kbits/sec
[  5] local 10.4.30.34 port 5001 connected with 10.4.30.35 port 45199
[  5]  0.0-30.9 sec  1.00 MBytes   272 Kbits/sec