Other Parts Discussed in Thread: UNIFLASH, CC3200, CC3100
What are the basic requirements for how to use UniFlash to load new binaries and support files into the CC3200 flash? The only way I feel convinced that I have loaded a new build into flash is to do a Format, then a Program (with erase, update, verify checked for all files), then a Service Pack Update, but this feels terribly redundant. So what are the conditions under which one should do a Format? Program? Service Pack Update? My intuition would be that a Format should only be required once (e.g., in order to set up a FAT), a Service Pack Update should only be required if you (1) do a Format, or (2) want to actually replace the Firmware running on the network processor(?), and I should be able to do just do a Program (erase/update/verify) in order to load new application files. Maybe I just don't adequately understand what exactly happens on each of these operations and someone can please explain them to me in more detail and for the benefit of the community at large?