Hi,
I am trying to porting the TI WL18XX WIFI Driver in Android-JB on a IMX6 Sololite custom board based on IMX6SLEVK and I have facing some problems.
I am using the Android Jelly Bean of the IMX6SLEVK for my custom board with some changes I had made.
Already the Atheros WIFI if ported in Android Jelly Bean for IMX6SLEVK.
So i applied patches for the Android jelly bean for my custom board. But when i am compiling the Android JB , Only atheros Wifi code is compiled. TI WL18XX WIFI code did not compiled .
I also attached the TI WL18XX WIFI driver patch link in this post. Please find it.
I also attached the TI WL18XX WIFI driver patch link.
Here is the driver link.
https://drive.google.com/file/d/0B3MisRwllBAKT2pPdWFVaXNZLUU/edit
I am asking about My added ti wifi driver is not compiled,atheros wifi driver only compiled.
I need to change the makefile which is higher up in the hierarchy which decides what are the drivers to be included. I need to find that makefile. But i do not know where the file is located.
Or how can I find it.
And I just attached the compilation of the ../myandroid/hardware/imx/wlan only
here it is:
marudham@marudham-engine:/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan$ ls
Android.mk atheros CleanSpec.mk intel mac80211
marudham@marudham-engine:/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan$ mm
============================================
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=4.3
TARGET_PRODUCT=full
TARGET_BUILD_VARIANT=eng
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
TARGET_ARCH_VARIANT=armv7-a
TARGET_CPU_VARIANT=generic
HOST_ARCH=x86
HOST_OS=linux
HOST_OS_EXTRA=Linux-2.6.32-47-generic-x86_64-with-Ubuntu-10.04-lucid
HOST_BUILD_TYPE=release
BUILD_ID=JSS15J
OUT_DIR=out
============================================
make: Entering directory `/media/Android/imx6SLandroid/myandroid'
make -C hardware/imx/wlan/atheros/compat-wireless ARCH=arm CROSS_COMPILE=/media/Android/imx6SLandroid/myandroid/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi- KLIB=/media/Android/imx6SLandroid/myandroid/kernel_imx KLIB_BUILD=/media/Android/imx6SLandroid/myandroid/kernel_imx COMPAT_CURDIR=/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless clean
make[1]: Entering directory `/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless'
make[2]: Entering directory `/media/Android/imx6SLandroid/myandroid/kernel_imx'
/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/config.mk:91: "WARNING: You are running a kernel >= 2.6.23, you should enable in it CONFIG_NET_SCHED for 802.11[ne] support"
CLEAN /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless
CLEAN /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless
CLEAN /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/.tmp_versions
make[2]: Leaving directory `/media/Android/imx6SLandroid/myandroid/kernel_imx'
make[1]: Leaving directory `/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless'
mkdir -p out/target/product/generic/system/etc/firmware/ath6k/AR6003/hw2.1.1/
mkdir -p out/target/product/generic/system/lib/modules/
make -C hardware/imx/wlan/atheros/compat-wireless O=/media/Android/imx6SLandroid/myandroid/kernel_imx ARCH=arm CROSS_COMPILE=/media/Android/imx6SLandroid/myandroid/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi- KLIB=/media/Android/imx6SLandroid/myandroid/kernel_imx KLIB_BUILD=/media/Android/imx6SLandroid/myandroid/kernel_imx COMPAT_CURDIR=/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless
make[1]: Entering directory `/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless'
./scripts/gen-compat-autoconf.sh config.mk > include/linux/compat_autoconf.h
make -C /media/Android/imx6SLandroid/myandroid/kernel_imx M=/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless modules
make[2]: Entering directory `/media/Android/imx6SLandroid/myandroid/kernel_imx'
/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/config.mk:91: "WARNING: You are running a kernel >= 2.6.23, you should enable in it CONFIG_NET_SCHED for 802.11[ne] support"
LD /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/compat/built-in.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/compat/main.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/compat/compat-3.2.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/compat/cordic.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/compat/crc8.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/compat/compat_atomic.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/compat/compat.o
LD /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/built-in.o
LD /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/built-in.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/main.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/regd.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/hw.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/key.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath.o
LD /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/built-in.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/debug.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/debugfs_pri.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/hif.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/htc.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/bmi.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/cfg80211.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/cfg80211_btcoex.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/pm.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/init.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/main.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/txrx.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/wmi.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/wmi_btcoex.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/sdio.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/platform.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/softmac.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/wmiconfig.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/recovery.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/testmode.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/usb.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_sdio.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.o
LD /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/built-in.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/main.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/status.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/sta_info.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/wep.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/wpa.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/scan.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/offchannel.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/ht.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/agg-tx.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/agg-rx.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/ibss.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/mlme.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/work.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/iface.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/rate.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/michael.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/tkip.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/aes_ccm.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/aes_cmac.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/cfg.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/rx.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/spectmgmt.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/tx.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/key.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/util.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/wme.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/event.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/chan.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/led.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/mesh.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/mesh_pathtbl.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/mesh_plink.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/mesh_hwmp.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/pm.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/driver-trace.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/rc80211_pid_algo.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/rc80211_minstrel.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/rc80211_minstrel_ht.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/mac80211.o
LD /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/rfkill/built-in.o
LD /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/built-in.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/core.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/sysfs.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/radiotap.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/util.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/reg.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/scan.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/nl80211.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/mlme.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/ibss.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/sme.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/chan.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/ethtool.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/mesh.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/wext-compat.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/wext-sme.o
CC [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/regdb.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/cfg80211.o
LD /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/built-in.o
Building modules, stage 2.
/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/config.mk:91: "WARNING: You are running a kernel >= 2.6.23, you should enable in it CONFIG_NET_SCHED for 802.11[ne] support"
MODPOST 6 modules
WARNING: "ath6kl_recovery_hb_event" [/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko] undefined!
WARNING: "ath6kl_init_debugfs_pri" [/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko] undefined!
WARNING: "ath6kl_recovery_init" [/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko] undefined!
WARNING: "ath6kl_recovery_suspend" [/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko] undefined!
WARNING: "ath6kl_wmi_error_report_event" [/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko] undefined!
WARNING: "ath6kl_mangle_mac_address" [/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko] undefined!
WARNING: "ath6kl_recovery_resume" [/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko] undefined!
WARNING: "ath6kl_recovery_cleanup" [/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko] undefined!
WARNING: "ath6kl_recovery_err_notify" [/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko] undefined!
CC /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/compat/compat.mod.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/compat/compat.ko
CC /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath.mod.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath.ko
CC /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_sdio.mod.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_sdio.ko
CC /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.mod.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/drivers/net/wireless/ath/ath6kl/ath6kl_usb.ko
CC /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/mac80211.mod.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/mac80211/mac80211.ko
CC /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/cfg80211.mod.o
LD [M] /media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless/net/wireless/cfg80211.ko
make[2]: Leaving directory `/media/Android/imx6SLandroid/myandroid/kernel_imx'
make[1]: Leaving directory `/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan/atheros/compat-wireless'
out/host/linux-x86/bin/acp -fpt hardware/imx/wlan/atheros/compat-wireless/compat/compat.ko out/target/product/generic/system/lib/modules/
out/host/linux-x86/bin/acp -fpt hardware/imx/wlan/atheros/compat-wireless/net/wireless/cfg80211.ko out/target/product/generic/system/lib/modules/
target Prebuilt: ath6kl_sdio.ko (out/target/product/generic/obj/ETC/ath6kl_sdio.ko_intermediates/ath6kl_sdio.ko)
Install: out/target/product/generic/system/lib/modules/ath6kl_sdio.ko
make: *** No rule to make target `out/target/product/generic/obj/lib/crtbegin_dynamic.o', needed by `out/target/product/generic/obj/EXECUTABLES/wlconf_intermediates/LINKED/wlconf'. Stop.
make: Leaving directory `/media/Android/imx6SLandroid/myandroid'
marudham@marudham-engine:/media/Android/imx6SLandroid/myandroid/hardware/imx/wlan$
Please find it.
i need to change the makefile where the atheros wifi driver is included in the Android BSP (JB), that is Android BSP (JB) is given by freescale. I want to change atheros to ti wl18xx .
Please kindly suggest any ideas to overcome this issue.
thanks and regrds,
vinothraj