This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL18xx and low rx bitrate

In STA mode, we have never seen that the rx bitrate (observable through 'iw wlan0 station dump') has been higher than 65.0 MBit/s MCS 7. This mode is maximum if using one antenna. However, we have two antennas mounted and the appropriate settings in wlconf (wl18xx.phy.number_of_assembled_ant2_4=0x02, wl18xx.ht.mode=0x00).

The tx bitrate, however, is often > 100 MBit/s.

How come the rx bitrate is so low? Are we missing some configuration?

It has been the same with a lot of different APs and firmware versions.

We're currently running firmware Rev 8.2.0.0.224, Rev 8.9.0.0.31.